Cancel
Showing results for 
Search instead for 
Did you mean: 

Importing graphic failed

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi

I am trying to import a STEP-file but I get the following message:

 

Untitled.png

 

The file is 491 MB and is exported from Solid Edge. Do you know what can be causing this problem?

I am using Plant Simulation 12.2.2

 

Thank you!

2 REPLIES 2

Re: Importing graphic failed

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Toobor,

I guess the file is too big and therefore cannot be converted.

But Solid Edge can also export our native format JT. This is always the preferred solution if available.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.
Highlighted

Re: Importing graphic failed

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thank you for your answer! It was that I suspected.