Cancel
Showing results for 
Search instead for 
Did you mean: 

Inaccuracy in table management

Builder
Builder

Hi there!

 

I was recently discovering an inaccuracy in the PlantSimulation x.y table management.

 

The situation is as follows:

If a row index of a table is first activated and a name for the header is given, the name still remains and is found even when the row index is deactivated later.

 

PlantSimulation is always looking from colum zero even when thre is no row index.

 

Earlier versions of PlantSimulation were reporting an error, PlantSimulation 12 just ignores the table properties.

1 REPLY

Re: Inaccuracy in table management

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Mak,

 

this was a change in 11.3.

 

Since then setCursor has a boolean return value which is true if the cursor could be set.

Otherwise it is false and the current cursor position is not changed.

 

This was a request of a customer who wanted to get rid of an additional test.

 

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.