Cancel
Showing results for 
Search instead for 
Did you mean: 

Inclined conveyor

Creator
Creator

Hello all!

 

What should I do to create an inclined conveyor?

2 REPLIES

Re: Inclined conveyor

Valued Contributor
Valued Contributor
mark the conveyor in 3D, right mouse click - show segments
mark one of the marker - hold the ALT key down and press the up key (direction keys)
you can also edit the segments table and insert the Z value (right mouse click - edit segments)

Re: Inclined conveyor

Siemens Phenom Siemens Phenom
Siemens Phenom

You do not have to first create a flat coveyor, though. You can set the height of the conveyor's anchor points already during its creation in the definitions dialog that opens when you click on the conveyor in the tool box. (This obviously does not work that way if you insert it using drag & drop since in that case the conveyor is already created once you release the mouse button over your frame).

In the definitions dialog, you can set the parameters of the next polycurve anchor, as e.g. a curve radius or, as in this case, the height of the next anchor.

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution