Cancel
Showing results for 
Search instead for 
Did you mean: 

Increasing capacity

Experimenter
Experimenter

Hello.

I am new to plant simulation. I would need some help. I have some working station. At this working stations the capacity can be 4. But I don t finde and possibility to change the capacity from 1 to 4. 

I tried it also with buffer, but in this case the entities are stored only until they reach the number of 4. And then only 1 entity is going to the working station.

Can pls somebody tell me how to increase the capacity?

 

Thanks

1 REPLY 1

Re: Increasing capacity

Builder
Builder

Hi izlop

 

You can use a parallel Proc to increase the capacity of the station and modify the same parameters.The buffer store the parts until the next station is free. In the toolbox, you can find the Parallel Proc.

 

Regards

Charly