Cancel
Showing results for 
Search instead for 
Did you mean: 

Initializing custom MUs in buffer with name

Creator
Creator

Hi,

 

In my model, the source produces two different types of MUs according to a table:

 

MU: .MUs.Type1 | Amount: 2 | Name: Product1

MU: .MUs.Type2 | Amount: 1 | Name: Product2

 

Following are 2 assembly stations - 1 buffer - 2 assembly stations. There are two workers.

 

At Station4, processing times are supposed to differ as follows:

 

MU-Type: Product1 | Time: 50.0

MU-Type: Product2 | Time: 1:10.0

 

With the init-Method, I want to set 1 of Product1 in the buffer, so that Worker2 starts working at Station3 straight away.

 

But when using

.MUs.Type1.create(Buffer)

as soon as the part reaches Station4, there is an error saying there are "no custom processing times specified for Type1". Entering processing times for ".MUs.Type1" in the ProcTable doesn't help.

 

-> Is there a way to name the part in the buffer?

 

I've tried the following code, but am getting an error message at "is" already Smiley Frustrated

is
teil: object;
do

teil:= .MUs.Type1.create(Buffer)
teil.setName(Product1)

end

Cheers,

Peritectic

 

2 REPLIES

Re: Initializing custom MUs in buffer with name

Phenom
Phenom

where did you get this piece of code (e.g. teil.setName(...)) from ?

 

It doesn't exist in SIMTALK

 

try

 

is
teil :object;
do

teil:= .MUs.Type1.create(Buffer);

if teil /=VOID then
teil.Name:="Product1";
end;

end;

Re: Initializing custom MUs in buffer with name

Creator
Creator

Thanks for the solution, simulator, it worked like a charm! Had to adjust it for Plantsim 13 to

 

var teil :object;

teil:= .MUs.Type1.create(Buffer)

if teil /=VOID then
teil.Name:="Product1"
end

Indeed, I don't know any SimTalk (just started a couple of days ago). I was looking for a method that might work via 'right click - show attributes and methods' and it appeared on the list for the MU.

 

So apparently my mistake was "only" using the wrong syntax (I'm testing Plantsim 13 at the moment). It works when written in the same format as above:

 

var teil :object;

teil:= .MUs.Type1.create(Buffer)
teil.setName("Product1")