Cancel
Showing results for 
Search instead for 
Did you mean: 

Installation error

Experimenter
Experimenter

Hello Everybody, I downloaded academic Plant Simulation version. When I tried to install the program appeared "this installation package is not supported by this processor" message. What do I should do to finish the installation?

Thanks for your help!

3 REPLIES

Re: Installation error

Siemens Phenom Siemens Phenom
Siemens Phenom
Hello Pranjal,
It seems that you're running a 32-bit version of Windows. The latest versions of Plant Simulation are 64-bit applications which need a 64-bit version of Windows.
Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Installation error

Experimenter
Experimenter
Yes I am using 32 bit operator. Does plant simulation software is available for 32 bit operating system?

Re: Installation error

Siemens Phenom Siemens Phenom
Siemens Phenom
No, we no longer support 32-bit Windows, since 32-bit only allows to use 4GB of main memory. Most machines you buy today have 8GB or more, so you want to be able to use this memory in your simulation models.
Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.