Cancel
Showing results for 
Search instead for 
Did you mean: 

Integration of different modules into 1 model in Plant Simulation

Experimenter
Experimenter
Hello!

Recently I have been using other simulation software for Plant Designing. Due to its limitations, just downloaded 30 days trial of "Tecnomatix Plant Simulation 11". Before purchasing, I would like to know that can we integrate different modules of a Plant into one single model?

My one module represents say -Raw material Ware Housing.
2nd module- Pre-batching& Mixing process
3rd -Packaging area

Can these 3 different modules be designed separately and added in one single libraray and later can be dragged in one single model. How is the feasibility ?

Waiting for your valuble reply.

Vivek
1 REPLY 1

Re: Integration of different modules into 1 model in Plant Simulation

Siemens Phenom Siemens Phenom
Siemens Phenom
Hello,
you can save each of the different models as an object into a file (Class Library -> Right Click -> Save As Object...).
Then you load these objects into a new model and insert each of these sub models as an instance into an empty frame.
Now you have a combined model.
Regards,
Ralf
Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.