Cancel
Showing results for 
Search instead for 
Did you mean: 

Interaction between failure importer and broker

Legend
Legend

Hello,

I'm trying to create a model where a machine has different failure profiles. Each profile must call a different worker.

In the example I've done, I have two profiles and two workers.


Everything works until I switch the workerpool to "paused" or "unplanned" (that's for manually simulate a worker not available when a machine request him).

In this case, the machine continues to work without requesting workers. It seems the failure importer is not requested.

You can find the model attached.

 

Regards,

Alessio

 

4 REPLIES 4

Re: Interaction between failure importer and broker

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Alessio,

 

Sorry, there is a bug in the software when a second failure starts during the station is waiting for a paused repair worker. This bug leads to repairing without worker.

The bug will be fixed in the next maintanance release.

 

Thanks for reporting the bug.

 

Kind regards

Karola

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Interaction between failure importer and broker

Legend
Legend

Ok,

I suppose future release will be avaiable for V12.xx only, isn't it?

Regards

Alessio

Highlighted

Re: Interaction between failure importer and broker

Siemens Phenom Siemens Phenom
Siemens Phenom

you are right, future releases will be available for V12.xx only.

 

Regards

Karola

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Interaction between failure importer and broker

Legend
Legend
Thank you for your information. Regards Alessio