Cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any way to realize random storage time in VSM library

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello GG and other experts,

        I want to model a store that can retrieval products in a range of time, such as 1 days to 2 days, just like rework station, but the capacity of rework station is just 1.

        or just like the basic object ParallelProc, we can set parameter of proctime to type distribution.

        Thanks very much.

3 REPLIES

Re: Is there any way to realize random storage time in VSM library

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Dongshui558,

 

this is not an object defined by the VSM theory, so you have to implement yourself.

Sorry.

 

Regards

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Re: Is there any way to realize random storage time in VSM library

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello GG,

       Thanks for your answer, can you share some information on how to build new objects which can intergated with VSM library. Up to now, VSM library is encrypted perfectly!

 

Re: Is there any way to realize random storage time in VSM library

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Dongshui8558,

 

it is a very hard task to create new objects running with the VSM library. So this is not possible for customers.

 

If there are any requirements for a new object which is also part VSM theory, we will decide whether to implement this object or not.

 

Reagrds

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution