Cancel
Showing results for 
Search instead for 
Did you mean: 

Large Scale Model - Using Google Earth/Maps

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Forum

I am trying to set a map of an area (multiple kms) for a background image but due to the scale it has very bad resolution.

I have inserted it as a tile to display in 3D (image below) and was wondering if there is a better way to get higher resolution images of large areas into Plant Simulation?

Regards,

HCapture.JPG

2 REPLIES 2

Re: Large Scale Model - Using Google Earth/Maps

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Hermias,

you need to find a way to get a bitmap with more pixels.
Plant Simulation remain that resolution.

Regards,

Peter

Re: Large Scale Model - Using Google Earth/Maps

Siemens Phenom Siemens Phenom
Siemens Phenom

Maybe Google Maps support has a way to create larger-resolution images.

To my knowledge, there is a developer interface to Google Maps, say, for applications that want to integrate Google Maps in some way, so I would guess, there at least exists a way to export images from Google Maps in a user-defined manner with more possibilities to configure the output.

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution