Cancel
Showing results for 
Search instead for 
Did you mean: 

Licence problems

Experimenter
Experimenter

Hey,

 

I am using plant simulation 9, because i have to make changes to an old model. This went fine, but I got another computer at the firm and I cannot get the licence file (Wibu key) activated in my new computer. My old computer was working on windows 7, my new computer on windows 8.

I use a research licence.

 

Does somebody know how to get the licence file working.

 

Thanks for the answeres.

 

Chris

3 REPLIES 3

Re: Licence problems

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello CODK89,

 

it's important to install the WIBU drivers for your WIBU key.

 

They are on the Plant Simulation DVD or you can download them from www.wibu.com.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Licence problems

Experimenter
Experimenter

I have installed a wibu key driver but get still some error.

 

The error is shown in the attachment.

 

How do i deal with this

Re: Licence problems

Siemens Phenom Siemens Phenom
Siemens Phenom

The problem is that the hostid (WIBU ID) of the WIBU dongle which is attached to your system doesn't match the one mentioned in the license file.

 

I can see that you have two license files configured. Maybe one is for another WIBU ID?

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.