Cancel
Showing results for 
Search instead for 
Did you mean: 

Limit Pick-and-Place (robots) rotation angles

Pioneer
Pioneer

Hi community, I have a question about the rotation angle of the Pick and Places.

 

As you can see in the attached picture, I want to ensure that PickandPlace can ONLY move in the permissible area (Green one) and that the avoid area (Red one) be a forbidden territory to my robot (Let's suppose the robot can not rotate full 360° and I want the robot to "look-like" how it moves in reallity).

 

 

And if the case was the opposite, and I wanted to ensure that the Robot went from the "source" to "Station1" going through the "forbidden area" (Red one), how can I ensure that it won't take it along the green one?

 

 

 

 

 

Thanks a lot!

1 REPLY 1

Re: Limit Pick-and-Place (robots) rotation angles

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
the pickAndPlace will select for the rotation the shortest way. So you will not need a blocking angle for the first case; if you want to turn over the red area, you need to set the blocking angle between the two destination to block the short way.
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net