Cancel
Showing results for 
Search instead for 
Did you mean: 

Limit to one worker on an assembly station with two stores

Valued Contributor
Valued Contributor

Hello,

 

I would like to modelize an assembly station, the worker should take two types of parts from one store (in my exemple Screw1 and Screw2).

When I configure the Store Importer => Services I have not the possibility to set the  amount like on a Station.

The problem appears when I have two workers in my Workerpool, the Broker sends two workers on the store, please see this Screenshot:

 

sample.jpg 

 

Is there a way to configure the number of workers who should work at the same type on a Assembly station / store couple ?

Or should I write a specific importer piece of code on Simtalk to manage such use case?

 

Please find my model attached, thanks in advance, regards.

1 REPLY 1

Re: Limit to one worker on an assembly station with two stores

Valued Contributor
Valued Contributor

Thanks to Phenom for the tip, I used the services to manage this use case.

 

See these modified properties :

 

WorkerPool => Attributes => Workers => Creation Table

AssemblyStation => Importer => Processing => Services

Store => Importer => Transport => Services

 

Please see the attached model for the corrected sample.