Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Line/Arc Dialog Box

Valued Contributor
Valued Contributor

Hi all,

 

I am creating a logistics model and for that I have a copy of the TwoLaneTrack into my class library. What I want to do is whenever I drag and drop it into the frame, open the line/arc dialog box.

 

Is it possible to open that window via SimTalk? I couldn't find it on the help files.

 

Thanks

1 REPLY 1

Re: Line/Arc Dialog Box

Siemens Phenom Siemens Phenom
Siemens Phenom

Add the copy to a toolbar and insert its instances by clicking on the toolbar item and then in the frame. That way, the dialog will open automatically.

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution