Cancel
Showing results for 
Search instead for 
Did you mean: 

Lines with different speeds

Creator
Creator

Hello,

 

I have a simulation that has two lines with different speeds (first with 0.4m/s and the secont with , the strange thing happens when the second mu enters in the first line, it moves "jumping" in the line. Why does this happen? Is there somehow to "fix" it?

 

The simmulation is attached

 

Thanks

2 REPLIES

Re: Lines with different speeds

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
I guess it is only a matter of animation. In tab curve of the line you can set the value in the field
Animate every x-th pixel to 1 and increase the real time speed in the eventController.
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

回复: Lines with different speeds

Genius
Genius

Hi,Phcella!

     In my view,this phenomenon is normal ,just because the second line speed is too slow .i try to find way to improve it,however,it's hard to solve it.