Cancel
Showing results for 
Search instead for 
Did you mean: 

Loading Entities onto EOMs

Pioneer
Pioneer

Hello,

I'm using a transfer station to load entities onto a EOM on a track. So, if i set the TS processing time at 0:04 it runs perfectly, but if i set it 0:05 it just loads 2 EOMs then stops the simulation and show an error message saying: .Models.Frame.TSTATION_LOAD: Unload not possible, no space on target.

Do you know why is that happening?

2 REPLIES

Re: Transfer station failure

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

There are two sensors at position 0 of the EOM which trigger a method of the transfer station twice. This confuses the transfer station.

Please delete both sensors at position 0 of the EOM and then define in the dialog of the transfer station again the sensor at position 0.

Then the transfer station will work with all times.

 

Kind regards

Karola

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Transfer station failure

Pioneer
Pioneer
Thank you very much, i would never guess that.