Cancel
Showing results for 
Search instead for 
Did you mean: 

Loading Transporter with Transfer station

Creator
Creator

Hi everyone,

 

I'm having some trouble with the loading of a transporter via a transfer station. The transporter is 'created' using a time schedule on a track. It can have around 100 parts on it. The loading of the first two transporters happens without troubles, however after a while the simulation stops and the following message pops up:

 

Unhandled error in 'Transferstation.OnExit': Unhandled error in 'Transferstation.exitStation': Unhandled error in 'Transferstation.successfulExit': A 'void' cannot accept the method 'Finished'.

 

I don't know what the cause is, since the first 200 parts are loaded without problems.

 

Looking forward to you answers!

 

 

 

 

11 REPLIES

Re: Loading Transporter with Transfer station

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Michael,

 

can you post your model?

 

Hard to say what's going wrong without it.

 

It would also be good to know which version of Plant Simulation you are using.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Loading Transporter with Transfer station

Creator
Creator

Hi Ralf,

 

thanks for you quick reply. Confidentiallity makes it not possible to upload a model now. I should then adapt it first which will take some time.

 

About the version, I'm using Plant Simulation 10.1, since I received a license for this version.

 

Without the model it is not possible to give some hints?

 

Regards,

 

Michael

Re: Loading Transporter with Transfer station

Creator
Creator
I will post an adaptes version tomorrow!

Re: Loading Transporter with Transfer station

Creator
Creator

Here's a simplified model (now it happens after 5 loaded parts).

 

I'm looking forward to your reply!

 

Regards,

 

Michael

 

Re: Loading Transporter with Transfer station

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Michael,

 

this seems to be a bug in the transfer station.

 

It only happens when you have a buffer of type stack.

 

We will look into this.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Loading Transporter with Transfer station

Creator
Creator

Hi Ralf,

 

Thanks for you answer. How should I solve it?

 

Regards,

 

Michael

Re: Loading Transporter with Transfer station

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Michael,

 

I've attached a fixed version of the TransferStation library (10.1.9).

 

Replace the one you in your installation (usually in C:\Program Files\Tecnomatix\Plant Simulation 10.1\Libraries\Tools) with this one.

 

Then you have to update the one in your model using the library manager.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Loading Transporter with Transfer station

Creator
Creator

Thank you, Ralf. 

 

In general, I really appreciate that this forum actually 'works'! Really valuable!

Re: Loading Transporter with Transfer station

Pioneer
Pioneer

Hello,

 

I know this is an old post but I am going to give it a shot anyway...

 

I am having the same problem with my unload station but I am using version 12.01. Do you know where i can get an updated transfer station for my library?

 

Thank you in advance!

 

Kbohara14