Cancel
Showing results for 
Search instead for 
Did you mean: 

Loading a SingleProc within a network using the Gantry Loader

Experimenter
Experimenter

Hello everyone,

 

is it possible to load a Subnetwork that contains only one SingleProc (and TableFiles etc.) by using the Gantry Loader and his methods (withouth using "cont.move(Subnetwork.SingleProc))?

 

I have tried to use "PlaceMuAt(Subnetwork.SingleProc)" which results in the error "Y-Position 37 of the loader can not be achieved"
By adressing the Subnetwork (PlaceMuAt(Subnetwork)), in which I have a Single Proc aswell as an entrance and exit, it results in: an error at "Cranes.Internal.TargetPosition" occured. Method: 55, Line "Unknown designator MUAnimations".

 

Thank you very much,

Simon

6 REPLIES 6

Re: Loading a SingleProc within a network using the Gantry Loader

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
the problem is, that the gantry loader gets its position from the positions of the destination objects.
If you have other positions of the stations in the sub-frame, it results in wrong positions.
You can try to transfer the yPos and xPos values of the subframe to the station in the subframe (F8 - double click at the attributes). Then you can test the method PlaceMuAt again.
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Loading a SingleProc within a network using the Gantry Loader

Experimenter
Experimenter

Thank you for the answer Steffen,

 

I changed the position of the SingleProc so that its X- and Y-positions are identical to the position of the Subnetwork.

 

When running the simulation, the same error still occurs.

 

Thanks for your help,

 

Simon

Highlighted

Re: Loading a SingleProc within a network using the Gantry Loader

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And you station is located in the area of the gantry?

 

can you post the model?

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Loading a SingleProc within a network using the Gantry Loader

Experimenter
Experimenter

Yes, the station is located within the area.
See model attached.

Re: Loading a SingleProc within a network using the Gantry Loader

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

ok, the position is taken from 3D, so you need to change the position of the SingleProc in 3D (3D-Attributes), move the SingleProc to the position 0,0 (left upper corner). Then it works.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Loading a SingleProc within a network using the Gantry Loader

Experimenter
Experimenter

Thank you so much!