Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Loading parts on pallets with the aid of a TransferStation

Creator
Creator

 

Hey Guys,

 

I have a problem with my TransferStation. I have two Sources (one for Loads and one for Pallets) With the aid of a TransferStation I wanna load those parts onto pallets. (One Load goes onto one pallet) For the first pallet and load everything is fine, but when the second pallet arrives at the sonsor of the transferstation and should load the part nothing happens and all the other pallets in the model stop and don't move anymore. I have attached my model. 

 

Ich hope you can help me. 

 

Thanks in advance Smiley Happy

 

Best Regards

 

Unistudent89

2 REPLIES 2

Re: Loading parts on pallets with the aid of a TransferStation

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hello,

I updated the Umladestation object to version 12.0  and it worked fine. So if you can update your Plant Sim version or install 11.x patches it could work.

 

 update objecct version.png

 

Otherwise a workarround is:

If you select the "Accumulating" checkbox in the Förderstrecke1 line then the pallets will continue to move.

Regards!

 

 

Re: Loading parts on pallets with the aid of a TransferStation

Creator
Creator

 

Hey Christian,

 

thank you very much for your help. Now it's working.

 

Best Regards

 

Unistudent89