Cancel
Showing results for 
Search instead for 
Did you mean: 

MU orientation in 3D line.

Experimenter
Experimenter

Hello,

 

I need to change the orientation of the MUs transported by a conveyor band (line) in the 3D model. I tried to create a new animation path that contains the necessary rotation, it works, but I didn´t find a way to change the default animation path. 

Captura.PNG

 

Any help would be greatly appreciated.

 

 

 

2 REPLIES 2

Re: MU orientation in 3D line.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

you could also try the "Turnplate" object in this case. You could attach such one to your conveyor and set the rotation angle accordingly with it. Would that also work for your application? 

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution


Re: MU orientation in 3D line.

Phenom
Phenom

you can redirect the "default" path to a newly defined path

 

like this

 

conveyor._3d.MuAnimations.getAnimation("default").redirectTo("NewAnimationPath")