Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

MU stopped on a non-Accumulating Line

Valued Contributor
Valued Contributor

Hello,
I've found a problem in Plant Simulation using the attribute Stopped of a MU when it's modified on a Line not Accumulating.


When you stops a MU:

@.stopped := true;

The attribute currentSpeed of the Line is set to 0 m/s.

 

When the MU is unstopped:

@.stopped := false;

Attribute currentSpeed of the line remains set to 0 and no MU is moved till there's a state change (like a Fail, Pause, or Unplanned, etc.). Or when you click Apply on the property window of the Line.

 

Attached there's a little example that simulates the issue.
Plant Simulation version utilized 11.2.2

 

! Using version 10.x there's no this problem.

 

Is it possible to correct this annoying problem?

 

For anyone needing: a possible work-around is to stop directly the Line and unstop it when the needed conditions are met.

Or (I don't remember if it works correctly) reset the current speed enabling and disabiling Acceleration).

 

Of course it would be better to have the possibility to stop the MU directly without troubles, like in ver. 10.

 

Thank you Robot Happy

 

BD

99 little bugs in the code,
99 little bugs in the code.
Take one down, patch it around.
127 little bugs in the code...
1 REPLY 1

Re: MU stopped on a non-Accumulating Line

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello BugsDiscoverer,

 

this bug already is fixed. Please use the latest product update.

You can find the download link in the file menu in the submenu "help".

 

Regards,

Karola

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.