Cancel
Showing results for 
Search instead for 
Did you mean: 

MU user defined attributes

Pioneer
Pioneer

Dear community members,

 

I would create (to save a lot of time) processes with this feature:

 

Process Time ---> Formula ---> @.Time

 

Where Time is a User Define Attribute of the Entity.

 

Is it possible, maybe using a method, set it like a random number Normally distributed? Because if I set Data type "time" I can't use "z_normal".

Thanks

 

2 REPLIES 2
Highlighted

Re: MU user defined attributes

Siemens Phenom Siemens Phenom
Siemens Phenom

If I understand you correctly, you want to specify the processing time in the MU, but not as a constant, but as a random number.

 

You can do this by creating a user-defined attribute of data type 'randtime', which allows you to define a random number distribution. Then you need to call rollDice to generate a new random number. For example name the user-defined attribute "a" and enter the formula @.a.rollDice as processing time.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: MU user defined attributes

Pioneer
Pioneer

It works.

 

Thank you so much