Cancel
Showing results for 
Search instead for 
Did you mean: 

Maintenance for machine

Innovator
Innovator

Hi,

I have following layout. I want to show singleproc2 is down for maintenance(not failed) and change the color of the machine.Also during this time, the parts should not pass through the singleproc2. Instead should keep moving on the line. How to do it .?

Maintenance.JPG

4 REPLIES

Re: Maintenance for machine

Phenom
Phenom

Have a look at the attribute ResSetup ( =true/false)

 

and

 

SetUpOnlyWhenEmpty (=true/false)

 

 

Unbenannt.PNG

Re: Maintenance for machine

Innovator
Innovator

For the following layout:

1.I have one global variable for singleproc. I have set value to 0, and changed the color of singleproc to grey. In this scenario I don want the entity to go to singleproc. But should go to singleproc2 and singleproc1. Again if i set value to 1 and change the color of singleproc to green,then the entity should go to this machine. Without adding failure to singleproc, is it possible to do it in anyway.? @simulator

model1.JPG

Re: Maintenance for machine

Phenom
Phenom
yes, this possible.

With the station entranceLocked attribute

you can control which station is served.


Re: Maintenance for machine

Innovator
Innovator

@simulator Thanks Smiley Happy