Cancel
Showing results for 
Search instead for 
Did you mean: 

Make a station to stop processing a part

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi,

 

A station changes processing time in a entrance control (set to "before actions"). In the entrance control I want to wait until some conditions are met (using the waituntil command), and then the station should start processing the part.

 

Can this be achieved?

2 REPLIES

Re: Make a station to stop processing a part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
no, the entrance control is the wrong place for this. After moving the MU to the station, Plant Simulation calculates the finished-time of the MU.
If you want to delay the start of processing, you need to delay the movement to the station (e.g. exit control of the predecessor) or you include a helping place to model the waiting.
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Make a station to stop processing a part

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Thank you for the reply, it helped a lot and I now have a working functionality for it!