Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Making a graph of MUs time in system

Creator
Creator

Is it possible to output a graph or a table with a time stamp of how long each entity spend in the system from source to drain?

2 REPLIES

Re: Making a graph of MUs time in system

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Christian,

 

the standard report of a Drain in the HTML report will show some key indicators per part:

DrainStatistics.png

 

If this is not sufficient you can add an entry control to the drain and collect the arrival time of each part.

You can the use the attribute 'CreationTime' of a MU to calculate the time it spent in the system.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Making a graph of MUs time in system

Creator
Creator

Thank you very much :-)