Cancel
Showing results for 
Search instead for 
Did you mean: 

Measuring the flow time

Dear community,

 

i've one question regarding the measure of flow time in a line production; i've done a simple model of a conwip (constant work in process) line.

To use this tool i need to know how the whole time passed by the article along the line; i'll explain better.

The article enters in the line with a code and a fixed exit time; the articles goes through the production line and when it arrives at the end i need to compare the flow time with the fixed time on the card (it has to be lower or equal of course).

To do this i can use 

EventController.SimTime - @.CreationTime

but it's comparing just the beginning and the end.

If i want to know the passing of time step by step (seconds or minutes) how can i do that?

thanks.

 

1 REPLY 1

Re: Measuring the flow time

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
you can observe the attribute location and write a "logfile" for the MU (e.g. as userdefined attribute).
This is an example for workers, but it should also work for MUs (worker - observer method for the attribute location).

https://www.bangsow.eu/detail_en.php?id=692
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net