Cancel
Showing results for 
Search instead for 
Did you mean: 

Method and Attribute of ExperimentManager

Experimenter
Experimenter

Hello everyone,

 

I am doing several experiments with ExperimentManager. After defining all input, output parameters,I would like to start, reset the ExperimentManger with  Method

 

1) is
   do
       root.ExperimentManager.start;
   end;

2) is
   do
       root.ExperimentManager.reset;
   end;

I don't know why the first method works but the second one does not.

 

Also, I would like to write a method to  perform some statements after the experiment finish but  I cannot figure out which attribute of ExperimentManger triggers the next action after the experiment finish.

 

Thanks

 

1 REPLY

Re: Method and Attribute of ExperimentManager

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi KhoaPham,

 

there is an example, which can be opened via the Start page (Small Examples):

 

Category: Toole and optimization

Topic: Experiment Manager

Example: Studies by SimTalk

 

To start an experiment run perform the instructions:

ExperimentManager.resetWizard; 
Experimentmanager.Start;

If you want to catch the end of the experiment study you can use the User evaluation method. Open the dialog Advanced Settings in the menu Tools. In the method you can use an instruction like

 

if localExp = ExpTable.ydim and localRun = numRuns then

end;

 

Regards

Peter