Cancel
Showing results for 
Search instead for 
Did you mean: 

Method for Worker to Pick Up Container At Line?

Pioneer
Pioneer

Can a line sensor method be written for when the sensor is triggered, the item is stopped on the line and a worker is called to pick it up and drop it off at a buffer? Or is a transfer station required between the line and and a workplace? I'm not sure how to put togther such method with a worker. Thanks!

1 REPLY 1
Highlighted

Betreff: Method for Worker to Pick Up Container At Line?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Vmorr,

 

yes you can, but it is not an easy task.

First, define a special worker class which will not be mediated by Broker/Workerpool

In the INIT method (of workerpool) you have to set the worker to be not mediated:

if worker.class=.MyWorkerclass then
		worker.automaticMediation := false

from now on, you can use the sensor control to call the worker, remeber, you need a workplace for the sensor position:

 

worker.goto(worplaceOfSensor)

At the entrance control of the workplace, you set the destination for the part, move the part to the worker and move the worker to the destination workplace:

 

		part.destination := TargetStation
		part.move(worker)
		worker.goto(WorplaceOfTargetStation)

Hope this will help.

 

 

Regards

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution