Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Mixer: no consumption & infinte output issue

Creator
Creator

Hi all,

 

I have one MaterialTable defining all recepies. The rows are in random order as i added stuff along the way (this should not be an issue as I understand it).

 

Mixer input is from two tanks, one with IngA and one with IngB. The mixer should take a certain amount of each and output a finite amount of MixA, say 500 litres.

 

Issue: no matter how much of the ingredients I put in the two tanks, the mixer is able to produce an infinite amount. The amount it produces is simply limited by the volume in the MixA tank after the mixer. This output tank will be filled even if its volume is 1 000 000 litres and the two input tank has 5 litres.

 

Am I missing some fundamental setting? Thanks in advance

3 REPLIES 3

Re: Mixer: no consumption & infinte output issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
what is your intention? Do you want produce once 500 liters and terminate the simulation?
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Mixer: no consumption & infinte output issue

Creator
Creator
The intention in the end is to have a large series of stations continuously producing, detailed explanation:

The simulation begins with say 5 discrete boxes of raw material (X kg each). There are different ingredients in each box. These boxes' contents are to be put as available raw materials in tanks in the beginning of the factory.

The first mixer should consume these raw materials and produce MixA. MixA will then be continuously fed downstream to the next mixing process's buffer tank. There MixB will be produced together with MixA and other raw materials.

The model will include everything from supplier deliveries coming in (the boxes), to the final product coming out in the end of the factory.

So the concept is clear to me, but I have now put many hours in fighting the mixers to start consuming the raw materials that are in my tanks.

Re: Mixer: no consumption & infinte output issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

the mixer will first be loaded with materials regarding the receipt until the mixer is full. Then the procTime of the mixer is startet, after the procTime the mixer will release the complete content to the successor(s). After a recovering time the process starts anew, if you feed the mixer with material. The size of the tanks upstream of the mixer doesnt limit the output, the outflow material rate is more important (e.g. source --> deportioner --> tank).

Sometimes it is a matter of animation, switch the event controller to real time to observe the simulation. If you have only some elements in the simulation, the event controller will skip the processing time of the mixer and it "looks like" a continuous process.

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net