Cancel
Showing results for 
Search instead for 
Did you mean: 

Model is not working as per the expectation

Valued Contributor
Valued Contributor

Hi All,

 

In my attached model when i increase the buffer (WIP_1010) size from 10 to 20 the throughput of the model is dicreased.

When i set the buffer capacity as 10 the throughput is 3230. But when I set the buffer capacity to 20, the throughput is dicreased to 2780.

 

 

 

Regards,

Ibrahim.

 

2 REPLIES 2

Re: Model is not working as per the expectation

Siemens Phenom Siemens Phenom
Siemens Phenom
The statistic value in the EventController (StartStat) is set to 0. So the warm up (fill up) phase of the model is part of the simulation time. Increasing the buffer means, during the ramp up the model is able to place more parts in the buffer. So these parts will not be counted yet. My recommendation is to set the EventContollers values to End: 1:08:00:00 and Statistic: 8:00:00.

I already tried in your model, but because of a calculation you do, this will lead to a div/0, which needs to fixed by you.

Regards

Always consider using the AttributeExplorer!

Re: Model is not working as per the expectation

Valued Contributor
Valued Contributor
Hi Eventdebugger,

Thank you for your response.

I will try your suggestions in the model.


Regards,
Ibrahim.