Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Modeling a dual capacity robot

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
you can also set the angle to 90° and click 4 times, start at a position left top of the insert point and click counter clock wise 4 times, than connect the end of the track with the start with a connector; I checked it, it works well with 12.2.1
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Modeling a dual capacity robot

Valued Contributor
Valued Contributor

Ah cool, that works. Now I just need to finish going through and figuring out how your model works otherwise. Thanks!