Cancel
Showing results for 
Search instead for 
Did you mean: 

Modelling a wire coil with a dismantle station

Hello everyone,

 

my aim is to modell a wire coil that is the material supply for a following process in which one "wireA" and two "wireB" are being produced.

My initial approach for this was using an dismantle station which dismantles one complete wire coil into 1000 "wireA" and 2000 "wireB".

This works fine so far, but I need those wires produced in the order: 1 x wireA, 2 x wire B, 1x wireA, 2x wireB, and so on... until 3000 pieces of wire are taken form the coil (and the empty coin body can leave the dismantle station).

 

Does anyone have an idea of how to achieve this?

 

Best regards

2 REPLIES 2

Re: Modelling a wire coil with a dismantle station

Valued Contributor
Valued Contributor

Hello,

If I understand this well, it could be like this.
I did not use dismantle station but only SingleProc and entrance strategy on it.(with checked before actions).

 

Re: Modelling a wire coil with a dismantle station

Thank you for that advice. It definitly helped me!