Cancel
Showing results for 
Search instead for 
Did you mean: 

Move a Train with @.move

Experimenter
Experimenter

Hello I have a issue with my simulation. I need to move a train with SimTalk from one Lane to another. I read in the Help that it is not possible to move a Train with the argument @.move, but why? Actually, as Help says, it just work with the exit control of a lane, but that is not a option for me.

 

In the attached file you will realize it is simple, just a sensor on a track that calls a method with the function @.move (destination). The second transporter is hitched to the first one. If I unhitch the second one, the method works great but due to that transporter is not a tractor, it will not move.

 

Any suggestion?

3 REPLIES

Betreff: Move a Train with @.move

Gears Phenom Gears Phenom
Gears Phenom

It's not possible to move a whole train, which consists of multiple individual objects, with one move-action. What you would probably have to do is:

  • loop through the train,
  • unhitch all trailers,
  • insert all transporters/trailers individually to the new lane at specific positions,
  • stop the transporter there, so that the trailers can be re-hitch unto it,
  • and let the transporter continue as soon as the last trailer was re-hitched to the train.

Quite cumbersome, and of course you also have to ensure that there is enough free space on the target lane for all your transporters/tractors before moving them!

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!

Betreff: Move a Train with @.move

Gears Phenom Gears Phenom
Gears Phenom

Couldn't resist Smiley Wink Check out the attached example, not sure whether you can open it, though... In case you can't, here's the source code of my sensor-method:

(SensorID : integer; Front : boolean)
is
	rStartPos		: real;
	oDestTrack		: object;
	rTrainLength	: real;
	olTrain			: list[object];
	oTrailer		: object;
	oCheckMU		: object;
	
do
	-- target position on other lane
	rStartPos	:= 15;
	oDestTrack	:= Track_Drain;
	
	-- move individual vehicles, if not part of a train
	if not @.isTractor then 
		debug; 
		if not @.insert(oDestTrack, rStartPos) then debug; end; 
		return;
	end;
	
	-- train is at least as long as the tractor
	rTrainLength	:= @.MULength;
	
	-- get whole train
	olTrain.create;
	oTrailer		:= @.getRearWagon;
	while (oTrailer /= void) loop
		-- add to train list
		olTrain.append(oTrailer);
		
		-- add to train length
		rTrainLength	:= rTrainLength + oTrailer.MULength;
		
		-- get next trailer, if any
		oTrailer		:= oTrailer.getRearWagon;
	end;
	
	-- check that there is enough space for an insert
	.ModelObjects.DummyVehicle.MULength	:= rTrainLength + 0.001 * olTrain.Dim;
	oCheckMU := .ModelObjects.DummyVehicle.create(oDestTrack, rStartPos);
	if (oCheckMU = void) then
		-- not enough free space!
		debug;
		return;
	else
		-- enough space, delete the check-vehicle
		oCheckMU.delete;
	end;
	
	-- unhitch all trailers and insert them into other track, start at end
	for local i := olTrain.Dim downto 1 loop
		-- get trailer
		oTrailer	:= olTrain.read(i);
		
		-- unhitch from train
		oTrailer.unhitchFront;
		
		-- update (remaining) train-length
		rTrainLength	:= rTrainLength - oTrailer.MULength;
		
		-- move to destination track (leave a small gap, so that the collision-control will be called)
		if not oTrailer.insert(oDestTrack, rStartPos - rTrainLength - 0.001) then
			debug;
		end;
		
		-- restore trailer-velocity (seems to be set to zero after the insert...!?)
		oTrailer.speed	:= oTrailer.class.speed;
	next;
	
	-- move the tractor and let it wait until its train is completely re-hitched
	@.a_iTargetNumTrailers	:= olTrain.Dim;
	@.a_iNumTrailers		:= 0;
	if not @.insert(oDestTrack, rStartPos) then debug; end; 
	@.stopped				:= true;

end;

The tractor is stopped after being moved to the new track. In the collision-control of the trailers/wagons, I check whether the original train has been re-hitched completely, and then un-stop the tractor. That's "all".

Regards,
Alex

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!

Betreff: Move a Train with @.move

Experimenter
Experimenter

Thanks and sorry for the delay. I didn't use your solution but it helped me to develop my own. Basically what I was trying to do is to move a train within the same track when it collides with a stopped train. I realized that @.move doesn't work with trains so what is nessesary to do is to unhitch every cart, move it forward, and hitch again by itself.

My code seems like this:

var vagon:object
var tractor:object
var rearVagon:object
var i:length

i:=1.6
tractor:=@
//debug
if @.FrontMU.getTractor.stopped=true or @.FrontMU.getTractor.collided=true and @.IsTractor=true //and Ocupado=false
	if @.~.Ocupado=false
		@.unhitchrear
		vagon:=@.RearMU
		@.insert(@.getLane,@.~.TractorEntrega.FrontPos+8)
		
		repeat 
			rearVagon:=vagon.getRearWagon
			vagon.unhitchrear
			
			vagon.insert(@.getLane,tractor.FrontPos-i)
			
			vagon.speed:=1.1
			vagon:=rearVagon
			i:=i+1.6
			until rearVagon = Void
	end
end