Cancel
Showing results for 
Search instead for 
Did you mean: 

Move entities from pickandplace to transporter.

Experimenter
Experimenter

Hello everyone.

 

I'm trying to move an entity from an input conveyor to a Transporter (on a track). The pick and place can already take the entity from the input conveyor but I don't know why it can deliver the entity into the Transporter.

 

I'm using this code to move the entity to the Transporter but it doesn't work. What am I doing wrong? 

 

if @.LastStation = Line
?.setdestination(transporter:1)

end

 

Thank you all in advantage. 

Febronio.

1 REPLY 1

Re: Move entities from pickandplace to transporter.

Siemens Phenom Siemens Phenom
Siemens Phenom

The easiest way to solve this is by simply dragging the PnP robot onto the conveyor/track. When you do that you'll get a prompt asking you what the robot should do at that object (load part, pick part, drop part or unload part). Select the operation you want, adn a sensor will automatically be created in the object at the place where you dropped the robot.

 

The exit operation of the robot will also be changed to "Place part at sensor" or "Load part onto MU at sensor", depending on your choice.