Cancel
Showing results for 
Search instead for 
Did you mean: 

Moving MUs from a buffer in root network into an entrance of a sub frame

Valued Contributor
Valued Contributor

Hello Community,

I am moving parts from a buffer object from a root network into a subframe; 
aiming at the entrance object (root.Maho.E; Maho being the name of the subframe; E the name of the entrance object where I want to send the MUs).

Now, connecting these with the usual edge (Kante) does work;
however, using an exit strategy with the command
 @.move(Maho)

or respectively 
@.move(root.Maho.E) 
does not work accordingly, the MUs get stuck in my buffer, and not into the subframe as they should.

This is a beginners mistake ;-) please give me a hint what I did wrong, thank you very much!

1 REPLY 1
Highlighted

Re: Moving MUs from a buffer in root network into an entrance of a sub frame

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
you cannot adress the interface (Übergang) object; if you connected all with connectors and interface objects you can use just

@.move

or you adress the object in the subframe (e.g. Eingangspuffer)

@.move(root.maho.eingangspuffer) or @.move(maho.eingangspuffer)
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net