06-08-2018 09:44 AM
Hello Community,
I am moving parts from a buffer object from a root network into a subframe;
aiming at the entrance object (root.Maho.E; Maho being the name of the subframe; E the name of the entrance object where I want to send the MUs).
Now, connecting these with the usual edge (Kante) does work;
however, using an exit strategy with the command
@.move(Maho)
or respectively
@.move(root.Maho.E)
does not work accordingly, the MUs get stuck in my buffer, and not into the subframe as they should.
This is a beginners mistake ;-) please give me a hint what I did wrong, thank you very much!
Solved! Go to Solution.
06-08-2018 09:54 AM
Steffen Bangsow freelance simulation specialist web: www.bangsow.eu mail: steffen@bangsow.net | ![]() |