Cancel
Showing results for 
Search instead for 
Did you mean: 

Moving parts to buffer with method error

Pioneer
Pioneer

Hello,

 

I have a model that I am moving parts from a store to a buffer this works well until the procduct is reduced to 3 or 4 parts left in the store. Then I get an error message I am not sure how to fix this issue. I have attached screen shots of the error message and store table file. I can not attach the model do to it being a work related model.

 

Can someone please help. Thank you Smiley Happy

5 REPLIES

Re: Moving parts to buffer with method error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
the error message is missing in your picture (you find it in the foot-line of the Debugger)
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Moving parts to buffer with method error

Siemens Phenom Siemens Phenom
Siemens Phenom

as already mentioned by Steffen, it´s hard to say anything without having a chance to see the error message ...

 


Regards

Always consider using the AttributeExplorer!

Re: Moving parts to buffer with method error

Pioneer
Pioneer

 

Thank you for your quick response.

 

My apologizes I thought I captured the whole screen. I have attached another screen shot of the message.

 

What I have noticed is that the object that the method is looking for is in the table file but when it is being called the buffer is at capacity so can not move.

 

The error "Invalid value in methcall, argument 1" is displayed.

Thank you for your time.

 

Re: Moving parts to buffer with method error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I guess the delay for methcall becomes negative, because the value in the table is lower than simTime, you Need to check the value in the table housingPB1[1,2] when the Debugger opens.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Moving parts to buffer with method error

Pioneer
Pioneer

Thank you that was the problem Smiley Happy