Cancel
Showing results for 
Search instead for 
Did you mean: 

Multi Portal Crane

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi All,

 

Does anyone has a model where 2 Portals are used to move a single part? Thanks!

Best Regards,
Paulo Araujo
4 REPLIES

Re: Multi Portal Crane

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

The Cranes library can handle multiple portals of a crane. Currently we can not synchronize two portals for carrying one part.

Re: Multi Portal Crane

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Dear Mr Guido,

 

I see this post is quite old.

 

I also now have to build a model where a 2 crane's are used to move one part.

 

Has the library changed? can one do this know?

 

If yes = do you have an example for me?

If no = do you know of a way around this? another way I could model this situation?

Re: Multi Portal Crane

Creator
Creator

Hi 

I also have the same problem, i don´t know how to syncronize two cranes to carry one big part. 

 

Please someone help me.

 

Thanks

 

Re: Multi Portal Crane

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

I do not know how to do this without changing the logic inside the crane.

 

I have managed to synchronize two cranes to move 2 parts at the same time. By modifying just the 3D-graphic you should be able to make it look like two cranes moving one part.

For example, you could make the Source1 and Buffer1 invisible, move the 3D-graphic of Source and Buffer a bit down etc. I uploaded two models, one with just the logic, and one with some modified graphics.