Cancel
Showing results for 
Search instead for 
Did you mean: 

Multi-level Experiment Manager issues while generatedesign experiments

Builder
Builder

Hi all,

 

I have filled the output, input and the parameters for each variable (lower,upper and step).

my variables are integer, so lower, upper and steps are integers too.

 

But, while generate the design of my experiments an error occures and I don't know why...

Is it because the number is too high ? I don't know why the loop works for k from 1 to 15 and at k=16 it doesn't.... (see below)

 

Any idea ?

 

ScreenHunter_16 Feb. 11 22.59.jpg

4 REPLIES 4
Highlighted

Re: Multi-level Experiment Manager issues while generatedesign experiments

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Flo_M,

 

you used a General Experimental Design.

You are right, the resulting number of experiments (variable nExp of type integer) is too high:

 

661500000 * 5 = 3307500000 > 2^31 – 1 = 2147483647 = maximum value for an integer variable.

 

Of course, such a debugger call should not happen.

We will adequately treat it.

 

In my opinion such large experiment study is not reasonable.

 

Regards,

Peter

Re: Multi-level Experiment Manager issues while generatedesign experiments

Builder
Builder

Hi Peter,

 

Thanks god, I spent 3 hours yesterday to understand where I make a mistake ^^

 

Of course it's not a reasonable, but I just wanted to auto-set my experiment manager and i didn't specially took into acount the number of experiments with my fake data... Robot Frustrated

 

Thanks for the answear !

It's good to knwo that 2147483647 is maximum value for an integer variable.

Where can I find all the data type limitations ? (i.e. number of charac, characters type...)

 

regards,

 

Flo-M

Re: Multi-level Experiment Manager issues while generatedesign experiments

Genius
Genius

The Help will help you Smiley Wink

use the index-search funktion and type "integer".

 

You will find an overview in the Reference Help --> SimTalk --> Datatypes

 

regards

 

Re: Multi-level Experiment Manager issues while generatedesign experiments

Builder
Builder

Thanks !