Cancel
Showing results for 
Search instead for 
Did you mean: 

Multi-manning problem - 2nd machine with 2 fixtures

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello all,

 

The model i am working on should behave as below, - I don't know whether i modelled it correctly or not.

 

1. Operator to Unload the 1st machine

2. Load the job on 1st machine

3. Inspect job - previous job

4. Load the 1st job on 2nd machine for first operation - drilling partA

5. Make sure the 1st machine not idle, in between if loading comes then unload/load the 1st machine 

6. unload the job on 2nd machine after 1st operation

7. Pushing the job to next fixture for next operation on same machine part B

8. inspection of 2nd job and wait till 2nd job comes on 1st fixture of second machine - partA

9.Load the second machine -as both the job are there. loading when 2 jobs loaded on 2 fixtures.

10. load /unload first machine 

11. unload both the job - both job will come out at same time - same processing time for both the operation at second machine.

12. Unload both the job - push 1st job from second fixture because it is ready .

13. push second job on fixture 2 from fixture 1 as only one operation is performed. and again wait for 3rd job to come to load both the jobs at the same time 

 

Attaching my model.

13.

3 REPLIES 3

Re: Multi-manning problem - 2nd machine with 2 fixtures

Phenom
Phenom

This is the third time you posted the same untouched model...

 

How about catching the anwsers to the posts and incorporating 

 

them accordingly in the model.

 

 

Re: Multi-manning problem - 2nd machine with 2 fixtures

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

 

I am having difficulty in modeling 2 machine scenario. Synchronisation of 2 jobs.

Re: Multi-manning problem - 2nd machine with 2 fixtures

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I meant second machine scenario.