Cancel
Showing results for 
Search instead for 
Did you mean: 

Multi portal crane - Pick part from Conveyor and Load to Buffer

Hello Guys,

I have a scenario where a Multi portal crane should pick part from a conveyor and store it on a buffer area. Buffer area can hold maximum 60 parts.

I have never worked on Multi portal crane and I am stuck with the model.

 

Appreciate help from experts.

4 REPLIES 4

Re: Multi portal crane - Pick part from Conveyor and Load to Buffer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
there are some examples in the example collection of Plant Simulation
category: Libraries

you should place a buffer place at the end of the line and load the part from there, so you have a defined position for pick up the part
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Multi portal crane - Pick part from Conveyor and Load to Buffer

Siemens Phenom Siemens Phenom
Siemens Phenom
have a look into the Recommendations of this forum (right side below the Tecnomatix Tech Tips)

Regards

Always consider using the AttributeExplorer!

Re: Multi portal crane - Pick part from Conveyor and Load to Buffer

Builder
Builder

Hi Mr. Steffen

Why is necessary place a buffer at the end of conveyor to perform the process?

Regards
Charly

Re: Multi portal crane - Pick part from Conveyor and Load to Buffer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

the portal crane calculates the coordinates of the objects dynamically. The conveyor as object has only one x,y,z-position and in many cases it doesn't meet the coordinate of the "placing" of the crane. Just test it.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net