Cancel
Showing results for 
Search instead for 
Did you mean: 

MultiPortalCrane - Energy Analyzer

Creator
Creator

Hello,

In my model I have a few groups of MultiportalCrane and I try to obtain energy consumption results.

Is it some possible to simulate energy consumption for MultiportalCrane ?
I can not see standard energy functions in the portal object window.
Could anyone help me to find easy/some solution for this issue ?

4 REPLIES

Re: MultiPortalCrane - Energy Analyzer

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Jsza,

 

the MultiportalCrane library is based on the Transporter object, which is not equipped with the Energy functionality. Therefore this evaluation is not available.

 

Regards,

Peter

Re: MultiPortalCrane - Energy Analyzer

Creator
Creator

Hello Peter,

 

 

OK, I understood. Direct functions are not available

but my question was, are there same other possibility ?

 

In SimTalk methods  for MultiPortalcrane I tray to use f.g.:

------------

 

.........

when 7 then
  
   ENhook.EnergyCurrentState:="Operational";
   portalObj.moveHook( 2);
   ENhook.EnergyCurrentState:="Off";

 

........

------------

 

where ENhook is the  "Standard" station as "motor" imitation

but it doesn't work correctly.


Could you or anybody suggest line of tought in this subject ?

 

regards

Re: MultiPortalCrane - Energy Analyzer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

you could use in the hook-object (tolley, portal) an observer for resWorking --> switch the power input of the energy state operational of a "dummy" object (powerInputOperational)

 

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: MultiPortalCrane - Energy Analyzer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have made a little example: you can detect the movement of the hook on the trolley object, the movement of the tolley on the portal and the portal movement on the crane. I have inserted observers in the trolley and portal in the subfolder MaterialFlow. For configuring the crane I have written a method, this you need only call once. The energy values i have defined in the dummy-objects (standby and working).

 

crane_energy.png

 

 

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net