Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple Gantt Wizard

Creator
Creator

Hello,

 

I have a problem with the GanttWizard. I want to use GanttWizard1 for SingleProc1 and GanttWizard for SingleProc. But after each simulation run, only one GanttWizard has collected data (see image attached).

 

What am I doing wrong? Can someone help me?

 

Thank you for your time and consideration.

 

Simulation model attached.

1 REPLY

Re: Multiple Gantt Wizard

Legend
Legend

Hello CLSC,

 

The GanttWizard is build to folow mu class and there location. When you associate a mu with a ganttWizard, it create some constructor and destructor method on the mu class.  If you associate an other ganttWizard to the same mu class the constructor and the destructor are overwritten and the first GanttWizards is unlinked.

 

For me there is no solution to your problem because the GanttWzards is not build to do that this way.

 

You have to use the ganttWizard this way :

first instance => several mu class,

second instance => several mu class but not the same

 

Regards,

 

rpinon