Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple Workers on a Workplace

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I don't think that the workplace is this detailed,  but say there is 20 people working at a workstation at one time can you combine the workplaces to have 20 workers at one workplace as opposed to having 20 individual workplaces for each worker?

 

Thanks

2 REPLIES 2

Re: Multiple Workers on a Workplace

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
the workplace is not connected to a specific worker (it is fixed assigned to a station). The capacity is one, so if you want to work with 20 workers at the same time at a station, you will need 20 workplaces.
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Highlighted

Re: Multiple Workers on a Workplace

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
You can consider the setting Workers can work remotely. Then you do no need Workplaces.

Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com