Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple Workers on a Workplace

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I don't think that the workplace is this detailed,  but say there is 20 people working at a workstation at one time can you combine the workplaces to have 20 workers at one workplace as opposed to having 20 individual workplaces for each worker?

 

Thanks

2 REPLIES 2

Re: Multiple Workers on a Workplace

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
the workplace is not connected to a specific worker (it is fixed assigned to a station). The capacity is one, so if you want to work with 20 workers at the same time at a station, you will need 20 workplaces.
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Multiple Workers on a Workplace

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
You can consider the setting Workers can work remotely. Then you do no need Workplaces.

Gert Nomden
Digital Factory Consultant
cardsplmsolutions.com