Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple products from a single source

Experimenter
Experimenter

Is it possible to create multiple products from a single source? For example, i'd like to manufacture 70 different products on a single line. And I'd like do it with a single source due to the restrictions of student version of Plant Simulation.

1 REPLY

Re: Multiple products from a single source

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
drag a tableFile into your frame, then
select in the source" MU selection" randomy or sequence and assign the table, now you can insert all MUs that you want to create into the tableFile (see also help)
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net