05-07-2015 05:39 AM
i was trying to solve the problem of manpower exactly as given in the examples.but i have multiple worker pools in my model and in the input of experiment manager.i changed the code in the advanced setting of experiment manager but it doesnt work.How can i solve the manpower problem with multiple worker pool as input ??
05-07-2015 10:48 AM
Can you post your method? If you use the manpower-example, than you need for each workerpool one table, and for each table at least one input value for the experiment manager.
Steffen Bangsow freelance simulation specialist web: www.bangsow.eu mail: steffen@bangsow.net | ![]() |
05-13-2015 07:02 AM
Hi steffen_B,
Its working, i made the copy of the same method given in the advanced setting of experiment manager 3 times,each for one workplace.the methods look like this..but any better way to do this ??
print "CONFIG Experiment ",localExp," use ",root.WorkerTab1[2,1]," workers1.";
root.WorkerPool1.setCreationTable(root.WorkerTab1);
print "CONFIG Experiment ",localExp," use ",root.WorkerTab2[2,1]," workers2.";
root.WorkerPool2.setCreationTable(root.WorkerTab2);
print "CONFIG Experiment ",localExp," use ",root.WorkerTab[2,1]," workers3.";
root.WorkerPool3.setCreationTable(root.WorkerTab3);