Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple workpool for different kind of workers.

Creator
Creator

Hi,

               I have this requirement where we have two control units of different type of workers (electrical, mechanical). Based on worktype required on each station, workers are pulled from these control units.

The model is taking input from a table file where the type of work required (electrical or mechanical) is available as an entry.

How can I configure my model to read the entry from table file and pull worker from accordingly from control unit (workpool)?

1 REPLY 1

Re: Multiple workpool for different kind of workers.

Siemens Phenom Siemens Phenom
Siemens Phenom

Create two (or more) workerpools and name them WPElec and WPMech. Create two brokers and name them BElec and BMech. Assign them accordingly ... done!

 

 


Regards

Always consider using the AttributeExplorer!