Cancel
Showing results for 
Search instead for 
Did you mean: 

Need Worker to carry parts from DismantleStation

Valued Contributor
Valued Contributor

Hi everyone,

 

I have a Worker problem. I need the worker to go to the DismantleStation, pick up an Entity (one of 4 Entities on a Container), to carry the Entity to a SingleProc, work there for 1minute and than go back to the DismantleStation to do the same again.

 

My Problem is that the Worker does not carry the Entity away. I think the main problem is that there is no option to set "Exit options" at a DismantleStation like you can do at a SingleProc.

 

Is there any solution for this problem?

(I cannot program so it would be great if the solution can be made by drag&drop or a TableFile maybe)

 

Thank You.

 

Best regards,

IceTea

1 REPLY

Re: Need Worker to carry parts from DismantleStation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You can insert a buffer (capacity=1) with the required strategy, to hold the parts that the worker should transport.


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com