Cancel
Showing results for 
Search instead for 
Did you mean: 

Need Worker to carry parts from DismantleStation

Experimenter
Experimenter

Dear Community, 

 

I need help for resolve a problem, I'm just a student trying to do a simulation for a class, I try to simulate a line of production where the workers pull up boxes at the end of the line and move it into pallets, i try to do this en plant simulaton but i can`t, somebody now how to do this?

 

I attached an image as an example.

 

Thanks

1 REPLY 1

Re: Need Worker to carry parts from DismantleStation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

several problems:

- you cannot load parts directly from the line, you will need to include some "pick up points" (e.g. SingleProc). The SingleProc supports the exit behavior "carry part away" (see help)

- if the destination is a place with a pallet on it, the worker will wait, until the place is empty; so you will need to trigger the movement of the part. This you can do in the entrance control of the workplace
e.g. @.cont.move(loadingPlace.cont)

- to trigger the transport of the empty and filled pallet, you can use a trick; set in all stations the exit behavior carry part away + add an empty exit control to this stations - so nothing happens in the first step; if you call now e.g. loadingPlace.cont.move --> the exit behavior is triggered and the worker is be called

here you find an example:

https://www.bangsow.eu/detail_en.php?id=763

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net